AN3815 - Software Files

For the software description refer to AN3815 on Freescale web site. 

Folder Structure: 

- Pixel_Board - Includes code for 56F8006 on the Pixel Board. ".mcp" file is the CodeWarrior project file. 

- Gateway_Board \
	- JM60-software - the s19 for the 9S08JM.
	- MC56F8006_Gate -  Includes code for 56F8006 the Gateway Board, ".mcp" file is the CodeWarrior project file.

- Serial App - Is a simple C# test application that sends commands over serial port to a set of 4 Pixel Boards.